Beli temperature data logger di monotaro.id
Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
- Hioki Temperature LoggerDeskripsi:A compact logger that can record temperature depending on the measurement target using an external sensor (sensor sold separately).It is small, lightweight, and pocket-sized so you don't have to worry about installation space.Two-item display that is easy to understand at a glance.Equipped with large capacity internal memory (60,000 data per channel).Data can be transferred to a PC without stopping recording.You can replace the battery while recording (recording continues for about 30 seconds even if the battery is removed).Since the previous recorded data is backed up, there is no need to worry even in the unlikely event of an incorrect operation.Purpose:For temperature measurement.For temperature control during transportation of pharmaceuticals, specimens, and chemicals.For temperature measurement and management in cold storage, storage, and showcases.For temperature control in inspection rooms, analysis/test rooms, factories, and kitchens.For temperature control of food, vegetables, fruits, and sweets.For fermentation and aging temperature control of foods such as alcohol, soy sauce, miso, and bread.
- Elitech Temperature Data LoggerDeskripsi:Elitech RC-5 USB Temperature Data Logger terutama digunakan untuk pencatatan suhu selama penyimpanan dan transportasi laut / udara / jalan raya bahan makanan, obat-obatan, bahan kimia dan produk lainnya, terutama banyak digunakan di semua jenis pergudangan, logistik dan rantai dingin, seperti wadah berpendingin, berpendingin truk paket berpendingin, penyimpanan dingin, laboratorium, dll. atau dalam bisnis rantai pasokan global berskala besar.Pencatat Data Suhu mini ini memiliki rentang pengukuran yang luas -30 ° C ~ + 70 ° C, akurasi tinggi, interval pencatatan yang dapat disesuaikan & masa pakai baterai yang lama untuk perekaman, pemantauan, dan analisis data suhu yang nyaman dan andal.Memiliki memori data permanen besar 32000 poin dan dilengkapi dengan perangkat lunak manajemen data untuk mengunduh data dengan mudah ke komputer melalui antarmuka USB. Dengan software ini, Anda dapat menganalisis data dalam bentuk tabel dan grafik dan mengekspornya dalam format gambar. Data dapat dipertanyakan, disimpan, dicetak dan diekspor dalam format Word / Excel / TXT / PDF.atribut:
- Temperature Resolution (°C/°F): 0.1
- ebro Temperature Data LoggerDeskripsi:With internal temperature sensorApplication samples• For process monitoring during convenience food production• For routine control in bedpan washers• For temperature mappings• To measure in raw material storage
- TESTO Mini Temperature Data LoggerDeskripsi:If your professional work involves food or pharmaceutical products, you know that the storage temperature of your goods should not exceed specific limit values under any circumstances. The testo 174T mini temperature data logger helps you comply with the specified temperature ranges. It records the temperature values reliably and thus ensures uninterrupted measurement data recording and documentation. This is what the testo 174T mini temperature data logger offers You can save up to 16 000 readings with the testo 174T temperature data logger securely. Because measurement data you have saved will not be lost even when the battery is empty or being replaced. This means a high level of data security is guaranteed. You can easily and quickly read the current temperature measuring value on its large display, along with any possible violations of limit values. The integrated NTC sensor stands for a high level of accuracy. Its large measuring range, from -30 to +70 °C, and its compact design make the testo 174T temperature data logger a competent support for virtually every kind of temperature recording.The testo 174T mini temperature data logger meets the requirements of EN 12830 and is HACCP-compliant, as well as having international HACCP certification, which means it is ideally suited for measurements in the food industry (e.g. for storage temperature measurement). Particularly practical: the data logger has water spray and jet protection according to IP 65. This enables it to be left in the measuring location even when warehouses are being cleaned. The temperature data logger is also suitable for temperature control in refrigerators or cold stores, because it can be used at temperatures down to -30 °C. Programming and analysis with the mini temperature data logger You can choose between three software versions for programming and reading your data logger and for analyzing the measurement data on the PC: ComSoft Basic software - available as a free download - for fast programming of the temperature data logger and easy data analysis ComSoft Professional software - can also be ordered as an option - offers a variety of possibilities for detailed analysis of temperature readings ComSoft CFR 21 Part 11 software - can also be ordered as an option - the best solution for special requirements according to CFR 21 Part 11 in the pharmaceutical sector You need a USB interface for programming and reading the mini temperature data logger.Attention: Please download the newest software version before using the USB interface for the first time. The software can be found in the download area. Product Includes: testo 174T mini temperature data logger, including wall bracket, batteries (2 x CR 2032 lithium) and calibration protocol.Monitoring and documentation of the temperature in cold rooms Many foods and drugs have to be stored within a specific cold temperature range. This can be done in individual cooled store rooms, but also in specialised cold stores or cold warehouses with high-rack facilities. The temperature must be continuously documented in all these cold storage facilities, because strict rules apply to quality management in both the food and drugs industries.Data loggers are usually installed at the so-called critical control points (CCPs) of the cold room, in order to identify any possible temperature deviations and to introduce appropriate countermeasures. Critical points are for instance doors or passages through to other temperature areas within a warehouse. Monitoring and documentation of transport temperature For all goods which react sensitively to temperature fluctuations or have to be stored within a predefined temperature range, uninterrupted measurement data recording and documentation play a major role.Incorrect temperature conditions during transport can lead to major losses of quality, including the total loss of value of the products that require monitoring.Using a data logger, shipments can be checked for compliance with the specified temperature ranges and the data can then be read, analysed and archived by means of special software. Monitoring the temperature in deep-freeze rooms for food There are many facilities where (deep) frozen foods need to be stored. These range from individual deep-freeze rooms at small food producers (e.g. butcher's shops), restaurants and supermarkets, via deep-freeze rooms in the food processing industry, right through to specialized refrigerated warehouses/high-bay deep-freeze warehouses. In all of these facilities, the temperature has to be documented continuously. Only temperature recording devices that comply with EN 12830 are allowed to be used in Europe. Data loggers are typically used to measure the air temperature in storage facilities of this kind. The measuring instrument is positioned in the deep-freeze room, where possible at critical locations, such as doors or refrigeration units, where it records temperature data at specified intervals (typically: every 15 minutes). The recorded data can subsequently be analyzed and archived using special software.atribut:
- Measuring Rate: 1 min - 24 h
- Memory: 16,000 Measuring values
- Operating Temperature: -30 to 70 °C
- Protection Class: IP65
- Battery Life: 500 days (15 min Measuring cycle, +25 °C)
- Battery Type: 2x3V button cell (CR 2032)
- Channels: 1 internal
- Dimensions (mm): 60x38x18.5
- Product Color : White
- Product/Housing Material: Plastic
- Standards: EU-guideline 2014/30/EU; 2011/65/EU
- Storage Temperature: -40 to +70 °C
- Weight (g): 35
- Elitech Digital Temperature and Humidity Data Loggeratribut:
- Temperature Range (°C/°F): -40 to +85/-40 to 185
- Humidity Range (%RH): 0 to 100
- Resolution (°C/°F/RH): 0.1; 0.1
- Record Capacity Temperature (points): 16000
- Logging interval: 10 seconds to 24 hours
- Data Interface: Micro USB
- Alarm Configuration: Buzzer; LCD Display
- Certification: EN12830, CE, RoHS
- Dimensions (mm): 118x61.5x19
- Logging Mode: Stop when full; Circular logging
- Power Supply: Single-use 3.6V ER14505H lithium battery; Or powered via USB
- TESTO Temperature and Humidity Data LoggerDeskripsi:Are the prescribed humidity and temperature values in warehouses and buildings being adhered to? Is mould in the apartment the result of insufficient ventilation, or caused by building damage? With the data logger for temperature and humidity testo 176 H1, you can find out.Up to two temperature and/or temperature/humidity probes can be connected to the 4-channel data logger testo 176 H1 and positioned in the room according to the individual requirements. A wide selection of probes is available to you for this purpose.The lock included in delivery protects your temperature and humidity loggers from unauthorized access.Security and convenience at all levelsThe testo 176 H1 data logger for temperature and humidity guarantees high data security and reliable measurement results on the basis of modern measurement technology.In addition to the current temperature and humidity values, the data logger testo 176 H1 also shows the dewpoint in the display (when a temperature/humidity probe is connected). You can read programmed limit values, min. and max. values, limit value violations as well as the remaining battery life easily from the large display. It is therefore not necessary to read out the temperature and humidity logger to a PC in order to gain a quick overview.Thanks to the large memory for 2 million measurement values, and the battery lifetime of up to 8 years, you can read out the data much less often, even at a shorter measurement intervals. The standard battery (AA) can be easily exchanged at any time by the user.Programming and evaluation of the data logger for temperature and humidityFor the programming and readout of the data logger for temperature and humidity, as well as for the analysis of the measurement data on a PC, three software versions are available.ComSoft Basic software - available for free download - allows the fast programming of the data logger as well as easy data analysisComSoft Professional software - optionally available - offers you different possibilities for the detailed analysis of temperature and humidity valuesComSoft CFR 21 Part 11 software - optionally available - optimum for the special requirements of the pharmaceutical sector according to CFR 21 Part 11Caution: To program the temperature and humidity data logger, you require a USB cable which is not included in delivery. Transfer of the saved measurement data from the data logger to a PC takes place by USB cable or SD card - you can order both as optional accessories together with your testo 176 H1.Application areas for the temperature and humidity data loggerMonitoring and documentation of building climateMonitoring and documentation of storage temperature and humidityMould in an apartment: With the temperature and humidity data logger you can find out whether moisture and mould on ceilings and walls are the consequence of building damage or a sign of incorrect ventilation behaviour. Product Includes: 4-channel data logger for temperature and humidity testo 176 H1 with external probe connections (NTC/capacitive humidity sensor), including wall bracket, battery and calibration protocol.Mould in an apartment Damp ceilings and walls may be a result of structural damage. In most cases, however, it is a sign of improper ventilation. Once the mould appears inside a house, the tenant assumes that moisture has come in from outside. Numerous disputes have erupted because of the issue of who is liable for the mould damage. It is very difficult to determine who or what has caused mould: the inhabitants or defective building construction? The temperature and humidity data logger testo 176 H1 is ideal for measuring humidity in ceilings and walls. For the measurement,you connect both optional probes – temperature/humidity probe and wall surface temperature probe – to the humidity logger testo 176 H1, and save the measurement data over a longer period.You need the temperature/humidity probe in order to monitor the dewpoint of the indoor air. The wall surface temperature probe attached to the wall measures the surface temperature of the wall. The dewpoint distance determined from the dewpoint of the indoor air and the wall surface temperature provides information on whether the mould in the apartment is caused by insufficient ventilation or by structural damage. Please note that the optional software ComSoft Professional is necessary for the calculation of the dewpoint distance. Monitoring and documentation of building climate Temperature and relative humidity are crucial factors when it comes to assessing air quality and comfort levels in indoor areas, e.g. in workplaces. Both values can be monitored and documented over the long term using data loggers.They are also very well suited for checking ventilation systems or for assessing any building moisture which occurs.The use of special software means measurement configurations can be carried out individually and recorded measurement data can be both analysed and archived. Monitoring and documentation of storage temperature and humidity Correct compliance with storage temperature and humidity is an important prerequisite for the quality assurance of many products, e.g. in the area of food and pharmaceutical products.As a general rule, data loggers are used to do this. They automatically check and document the profile of the ambient conditions and thus make a crucial contribution to verifiable preservation of product quality.Viewing breaches of limit values directly on the display means you can respond quickly to temperature and humidity deviations. In addition, with the help of the configuration and read-out software, customer-specific measurement configurations can be carried out and recorded measurement data can be both analysed and archived.atribut:
- Interface: mini usb, SD card slot
- Product Color : Black
- Product/Housing Material: Plastic
- Standards: EU-guideline 2014/30/EU; 2011/65/EU
- Lutron SD Card Real Time Data LoggerDeskripsi:SD Card real time data loggerHUMIDITY/BAROMETER/TEMP.DATA RECORDERModel : MHB-382SD- Recorder with real time recorder, save the measuring data along the time information (year, month, date, minute, second) into the SD memory card and can be download to the Excel, extra software is no need.- Humidity : 10 to 90 %RH.- Temperature : 0 to 50.0°C- Barometer ; 10 to 1100 hPa, mmHg, inHg.- Show barometer, humidity and temperature value in the same LCD.- Large LCD display, easy readout.- Low power consumption and long battery life when use battery power.- DC 1.5V (UM-4, AAA) battery x 6 PCs or DC 9V adapter in.- RS232/USB computer interface.- Size : 132 x 80 x 32 m.- Patent: Taiwan, China, Japan, Germany, USA pending.atribut:
- Dimensions (mm): 132x80x32
- Fujita Waterproof Data Loggeratribut:
- Weight (g): 45
- Power: Coil type lithium battery (CR2477) x1 pieces (included)
- Dimensions (Width W x Depth D x Height H) (mm): 90x15x34
- Protection Level: IP67 (container)
- Data Memory (dots): (Temperature / humidity) each 16000
- Purpose of Use: For logistics of medical field/food related industry. Work environment settings for factories and others.
- TESTO Alat Perekam Data Suhu MiniDeskripsi:Jika pekerjaan profesional Anda melibatkan produk makanan atau farmasi, Anda tahu bahwa suhu penyimpanan barang Anda tidak boleh melebihi nilai batas tertentu dalam keadaan apa pun. Pencatat data suhu mini testo 174T membantu Anda mematuhi rentang suhu yang ditentukan. Alat ini merekam nilai suhu dengan baik dan memastikan perekaman dan dokumentasi data pengukuran tanpa gangguan.Perekam data suhu mini testo 174T memenuhi persyaratan EN 12830 dan sesuai dengan standard HACCP, serta memiliki sertifikasi HACCP internasional, yang berarti cocok untuk pengukuran di industri makanan (misalnya untuk pengukuran suhu penyimpanan). Alat ini memiliki perlindungan terhadap semprotan air dan pancaran air sesuai dengan standard proteksi IP65. Hal ini memungkinkan alat tersebut untuk tetap berada di lokasi pengukuran bahkan saat gudang sedang dibersihkan. Alat ini juga cocok untuk indikator untuk mengatur suhu di lemari es atau cold store, karena dapat digunakan pada temperatur di bawah -30 °C.atribut:
- Measurement Item: Temperature
- Container protection class: IP65
- Dimensions (mm): 38x18.5x60
- Measurement Temperature Range (°C): -30 to 70
- Minimum Temperature Display (°C): 0.1
- Number of Data Memory: 16000 data
- Power Supply: Lithium Coin Cell Battery (CR2032)x2 (accessory)
- Purpose of Use: Temperature change data is recorded. For monitoring temperature of display case and refrigerator.
- ebro Temperature LoggerDeskripsi:With a storage capacity of 40,000 measured values, the EBI 20 data loggers are used for continuous documentation and monitoring of temperature. All EBI 20 data loggers are supplied with a factory calibration certificate and a battery that can be replaced by the user. The data loggers are particularly impressive because of their good price-performance ratio. Applications:- Transport monitoring- Warehouse monitoring - Process monitoringatribut:
- Protection Class: IP67
- Dimensions (mm): 69x48x22
- Resolution: 0.1°C
- Battery: 3V Lithium (CR2450), exchangeable
- Measurands: Temperature
- Measurement Interval: 1min to 24 hours
- Measurement Range (°C): -30 to +70
- Storage Temperature (°C): -40 to +70
- TZONE Data Logger SuhuDeskripsi:- Original TZONE- Mendapatkan Sertifikat Kalibrasi berstandar NIST USA, dan CNAS- Plug and play, tanpa software: Otomatis memberikan laporan PDF/CSV- Temperature Data Logger yang ideal digunakan untuk pergudangan, logistik, ekspedisi, transportasi bahan makanan, obat-obatan, bahan kimia, cold storage , laboratorium, dll.atribut:
- Accuracy: +/- 0.5 C (-20 top 40 C), +/- 1 C (other range)
- Alarm Delay: Programmable (0 to 960 minutes), default: 10 minutes
- Alarm Range: Programmable high or low alarm limit for each channel
- Communication Interface: USB 2.0
- Default Temperature Alarm Range (°C): less than 2 or greater than 8
- Dimensions (mm): 89x36x16
- Interval: Programmable (10s to 18 h), default: 10 minutes
- Memory Capacity: 32000
- Recording Option: Push-to-start or Start Delay
- Resolution: 0.1
- Shelf Life/Battery: Typically 1 year, CR2032 3.0V Lithium battery
- Start Delay: Programmable (0 to 254 minutes), default: 30 minute
- Temperature Operating Range (°C): -30 to 60
- Temperature Scale: °C or °F
- Time Zone: UTC +0:00 (default)
- Waterproof Level: IP65 (with waterproof O-ring)
- ebro Single-Use Temperature Data LoggerDeskripsi:The EBI 330-T30 Single-Use USB Data Logger provides cost-saving continuous temperature monitoring during the transport of temperature-sensitive goods. The logger can easily be connected to any PC via the USB interface. Directly on the destination, the EBI 330-T30 creates a PDF report automatically with all the important data of the temperature curve. A special software is not required. The software by which the data logger can be read out is optional and FDA 21 CFR Part 11 compliant. Before using the EBI 330-T30 USB data logger can be programmed easily via the free online configurator at www.ebi330.com, a pre-configuration is also possible.Applications: Logistics, Laboratory, Pharma – Vaccine –Drugs, Food and Storage controlatribut:
- Data Memory: 20.000 (Measured Data)
- Accuracy (°C): ±0.5 (±0.8 °C for the remaining measuring range)
- Protection Class: IP65
- Dimensions (mm): 80x28x12
- Resolution (°C): 0.1
- Battery (V): 3 (CR2032)
- Measured Variables: Temperature
- Measurement Range (°C): -30…+60
- Storage Temperature (°C): -30…+60
- Extech Data Logger Suhu / Kelembabanatribut:
- Item: Data Logger
- Humidity Range (% RH): 0-100
- Temperature Range (°C): -40 to 85
- Resolution (%RH): 0.1
- Type: Temperature, Humidity
- Fujita NFC Watch Logger Internal/External Temperature Sensoratribut:
- Interface: NFC communication
- Item to be Measured: Temperature
- Temperature Accuracy (°C): Internal/±0.5, External/±0.3 (-10 to +50)/±0.5 (other)
- Size (mm): 90x15x34
- Temperature Resolution (°C): 0.1
- Accessories: External probe (P-1070)x1, CR2477 lithium batteryx1
- Display: LCD (measured value, under recording, cell remaining amount, warning)
- Measurement Interval: 1 - 255 (1 minute unit)
- Package Size (mm): 155x90x50
- Sensor: Internal, external
- Supported OS: Windows(R)XP/VistaTM/7/8
- Temperature Measurement Range (°C): -40 to +80
- Temperature Memory: 16000 data
- KIMO Temperature Data LoggerDeskripsi:KIMO Instruments Temperature Model KT 50When straightforward temperature readings are required, look no further than to the KT 50 Mini Data Logger. Data Loggers are widely used in agriculture, industry and clinical laboratories to monitor a variety of parameters.atribut:
- Battery Life (day): 500
- Display: 1-line display
- Height (mm): 21.9
- IP Protection: IP 65
- Length (mm): 61.3
- Magnetise Case: Yes
- Parameter: Temperature
- Power Supply: 2 x CR2032 (lithium 3V)
- Securable Mounting: A place for anti theft device
- Sensor: Internal sensors
- Standard: 2011/65/EU RoHS II, 2012/19/EU WEEE, 2014/30/EU EMC, 2014/35/EU Low Voltage
- Width (mm): 40
- KRISBOW Termometer Digitalatribut:
- Dimensions (mm): 165x76x43
- Type Input: Dual
- Temperature Range (°C): 20 - +1000
- Temperature Range (°F): 4 - +1832
- AND EnvIronmental Temperature and Humidity Meteratribut:
- Internal capacity: One
- Order Code: 57377285
- Product Number: AD-5685
- range of measurement: Temperature: 0.0 ° C to 50.0 ° C (minimum Display 0.1 ° C), relative humidity: 20% RH to 90% RH (minimum Display 1% RH)
- Measurement Item: Temperature, relative humidity
- Display Range: Heat stroke index: 0.0 ° C to 60.0 ° C (minimum Display 0.1 ° C), absolute humidity: 1g / m
- AS ONE Digital Thermo-Hygrometer Built-In Data Loggeratribut:
- Size (mm): 64x30x184
- Resolution (°C): 0.1 (0 - 200), 1 (other than the left)
- Body Temperature Accuracy (°C): -200 to +200 , 400 - 1370/±(0.3%rdg + 1), 200 - 400/±(0.5%rdg + 1)
- Function: Data logger (maximum 16000 data), data hold, temperature deviation, maximum/minimum value display, auto power off, battery exhaustion display
- Accessories: Beads type K thermocouple sensor TPK-01 x 2, RS-232C cable, software, Carrying case
- Display unit: Switching between Celsius and Fahrenheit
- Package Size (mm): 170x315x80
- Power Supply: 006P (9V) dry cell x 1 (test included) or AC adapter (optional)
- Sampling Time (s): 3
Daftar Harga temperature data logger Terbaru January 2026
| Hioki Temperature Logger | Rp3.099.900 |
| Elitech Temperature Data Logger | Rp429.900 |
| ebro Temperature Data Logger | Rp3.699.900 |
| TESTO Mini Temperature Data Logger | Rp2.199.900 |
| Elitech Digital Temperature and Humidity Data Logger | Rp1.099.900 |
| TESTO Temperature and Humidity Data Logger | Rp11.999.900 |
| Lutron SD Card Real Time Data Logger | Rp3.599.900 |
| Fujita Waterproof Data Logger | Rp2.399.900 |
| TESTO Alat Perekam Data Suhu Mini | Rp2.199.900 |
| ebro Temperature Logger | Rp1.899.900 |
Data diperbarui pada 23/01/2026 (Harga belum termasuk PPN)